Hi experts,
Met trouble to find a suitable device to support below requirement from my customer. please help to suggest thanks.
34V+/-10% input,
30V +/-5% output, 5~80mA ,
Short circuit protection,
OCP 110mA
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi experts,
Met trouble to find a suitable device to support below requirement from my customer. please help to suggest thanks.
34V+/-10% input,
30V +/-5% output, 5~80mA ,
Short circuit protection,
OCP 110mA
Hi Yue,
The closest we have is the LM317L-N.
While the current limit is not 110mA (we actually don't LDO's with a precision current limit), the unique aspect of the LM317L architecture is that it will thermally foldback the current limit to protect itself.
Figure 34 shows how you can force a maximum current limit:
Does this work for you? What is the background for the 110mA current limit?