This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ25155: Hi does TI provide driver sample C code for PMID bq25155?

Part Number: BQ25155

Hi does TI provide driver sample C code for PMID bq25155?

My company would like to use a driver sample code as a reference to develop our own driver for Nordic embedded system.

Thanks. Regards.

  • Hello,

    I've attached a driver.

    // SPDX-License-Identifier: GPL-2.0
    // BQ2515X Battery Charger Driver
    // Copyright (C) 2020 Texas Instruments Incorporated - http://www.ti.com/
    
    #include <linux/err.h>
    #include <linux/i2c.h>
    #include <linux/init.h>
    #include <linux/interrupt.h>
    #include <linux/kernel.h>
    #include <linux/module.h>
    #include <linux/of_device.h>
    #include <linux/gpio/consumer.h>
    #include <linux/power_supply.h>
    #include <linux/regmap.h>
    #include <linux/types.h>
    
    #define BQ2515X_MANUFACTURER "Texas Instruments"
    
    #define BQ2515X_STAT0		0x00
    #define BQ2515X_STAT1		0x01
    #define BQ2515X_STAT2		0x02
    #define BQ2515X_FLAG0		0x03
    #define BQ2515X_FLAG1		0x04
    #define BQ2515X_FLAG2		0x05
    #define BQ2515X_FLAG3		0x06
    #define BQ2515X_MASK0		0x07
    #define BQ2515X_MASK1		0x08
    #define BQ2515X_MASK2		0x09
    #define BQ2515X_MASK3		0x0a
    #define BQ2515X_VBAT_CTRL	0x12
    #define BQ2515X_ICHG_CTRL	0x13
    #define BQ2515X_PCHRGCTRL	0x14
    #define BQ2515X_TERMCTRL	0x15
    #define BQ2515X_BUVLO		0x16
    #define BQ2515X_CHARGERCTRL0	0x17
    #define BQ2515X_CHARGERCTRL1	0x18
    #define BQ2515X_ILIMCTRL	0x19
    #define BQ2515X_LDOCTRL		0x1d
    #define BQ2515X_MRCTRL		0x30
    #define BQ2515X_ICCTRL0		0x35
    #define BQ2515X_ICCTRL1		0x36
    #define BQ2515X_ICCTRL2		0x37
    #define BQ2515X_ADCCTRL0	0x40
    #define BQ2515X_ADCCTRL1	0x41
    #define BQ2515X_ADC_VBAT_M	0x42
    #define BQ2515X_ADC_VBAT_L	0x43
    #define BQ2515X_ADC_TS_M	0x44
    #define BQ2515X_ADC_TS_L	0x45
    #define BQ2515X_ADC_ICHG_M	0x46
    #define BQ2515X_ADC_ICHG_L	0x47
    #define BQ2515X_ADC_ADCIN_M	0x48
    #define BQ2515X_ADC_ADCIN_L	0x49
    #define BQ2515X_ADC_VIN_M	0x4a
    #define BQ2515X_ADC_VIN_L	0x4b
    #define BQ2515X_ADC_PMID_M	0x4c
    #define BQ2515X_ADC_PMID_L	0x4d
    #define BQ2515X_ADC_IIN_M	0x4e
    #define BQ2515X_ADC_IIN_L	0x4f
    #define BQ2515X_ADC_COMP1_M	0x52
    #define BQ2515X_ADC_COMP1_L	0X53
    #define BQ2515X_ADC_COMP2_M	0X54
    #define BQ2515X_ADC_COMP2_L	0x55
    #define BQ2515X_ADC_COMP3_M	0x56
    #define BQ2515X_ADC_COMP3_L	0x57
    #define BQ2515X_ADC_READ_EN	0x58
    #define BQ2515X_TS_FASTCHGCTRL	0x61
    #define BQ2515X_TS_COLD		0x62
    #define BQ2515X_TS_COOL		0x63
    #define BQ2515X_TS_WARM		0x64
    #define BQ2515X_TS_HOT		0x65
    #define BQ2515X_DEVICE_ID	0x6f
    
    #define BQ2515X_DEFAULT_ICHG_UA		10000
    #define BQ25150_DEFAULT_ILIM_UA		100000
    #define BQ25155_DEFAULT_ILIM_UA		500000
    #define BQ2515X_DEFAULT_VBAT_REG_UV	4200000
    #define BQ2515X_DEFAULT_IPRECHARGE_UA	2500
    
    #define BQ2515X_DIVISOR				65536
    #define BQ2515X_VBAT_BASE_VOLT			3600000
    #define BQ2515X_VBAT_REG_MAX			4600000
    #define BQ2515X_VBAT_REG_MIN			3600000
    #define BQ2515X_VBAT_STEP_UV			10000
    #define BQ2515X_UV_FACTOR			1000000
    #define BQ2515X_ICHG_DIVISOR			52429
    #define BQ2515X_ICHG_CURR_STEP_THRESH_UA	318750
    #define BQ2515X_ICHG_MIN_UA			0
    #define BQ2515X_ICHG_MAX_UA			500000
    #define BQ2515X_ICHG_RNG_1B0_UA			1250
    #define BQ2515X_ICHG_RNG_1B1_UA			2500
    #define BQ2515X_VLOWV_SEL_1B0_UV		3000000
    #define BQ2515X_VLOWV_SEL_1B1_UV		2800000
    #define BQ2515X_PRECHRG_ICHRG_RNGE_1875_UA	18750
    #define BQ2515X_PRECHRG_ICHRG_RNGE_3750_UA	37500
    #define BQ2515X_TWAKE2_MIN_US			1700000
    #define BQ2515X_TWAKE2_MAX_US			2300000
    
    #define BQ2515X_ILIM_150MA	0x2
    #define BQ2515X_ILIM_MASK	0x7
    #define BQ2515X_HEALTH_MASK	0xf
    #define BQ2515X_ICHGRNG_MASK	0x80
    #define BQ2515X_STAT0_MASK	0x0f
    #define BQ2515X_STAT1_MASK	0x1f
    #define BQ2515X_PRECHARGE_MASK	0x1f
    
    #define BQ2515X_TS_HOT_STAT		BIT(0)
    #define BQ2515X_TS_WARM_STAT		BIT(1)
    #define BQ2515X_TS_COOL_STAT		BIT(2)
    #define BQ2515X_TS_COLD_STAT		BIT(3)
    #define BQ2515X_SAFETY_TIMER_EXP	BIT(5)
    
    #define BQ2515X_VIN_GOOD		BIT(0)
    #define BQ2515X_CHRG_DONE		BIT(5)
    #define BQ2515X_CV_CHRG_MODE		BIT(6)
    
    #define BQ2515X_VIN_OVP_FAULT_STAT	BIT(7)
    
    #define BQ2515X_WATCHDOG_DISABLE	BIT(4)
    
    #define BQ2515X_ICHARGE_RANGE		BIT(7)
    
    #define BQ2515X_VLOWV_SEL		BIT(5)
    
    #define BQ2515X_CHARGER_DISABLE		BIT(0)
    
    #define BQ2515X_HWRESET_14S_WD		BIT(1)
    
    static const int bq2515x_ilim_lvl_values[] = {
    	50000, 100000, 150000, 200000, 300000, 400000, 500000, 600000
    };
    
    /**
     * struct bq2515x_init_data -
     * @icgh: fast charge current
     * @vreg: charge voltage
     * @ilim: input current limit
     * @iprecharge: precharge current
     */
    struct bq2515x_init_data {
    	int ichg;
    	int vreg;
    	int ilim;
    	int iprecharge;
    };
    
    enum bq2515x_id {
    	BQ25150,
    	BQ25155,
    	BQ21061,
    };
    
    /**
     * struct bq2515x_device -
     * @mains: mains properties
     * @battery: battery properties
     * @client: i2c client structure
     * @regmap: register map structure
     * @dev: device structure
     * @lock: thread lock structure
     * @id: enumeration of device ids
     *
     * @reset_gpio: manual reset (MR) pin
     * @lp_gpio: low power mode pin
     * @ac_detect_gpio: power good (PG) pin
     * @ce_gpio: charge enable (CE) pin
     *
     * @model_name: string value describing device model
     * @device_id: value of device_id
     * @mains_online: boolean value indicating power supply online
     *
     * @bq2515x_init_data init_data: charger initialization data structure
     */
    struct bq2515x_device {
    	struct power_supply *mains;
    	struct power_supply *battery;
    	struct i2c_client *client;
    	struct regmap *regmap;
    	struct device *dev;
    	struct mutex lock;
    	enum bq2515x_id id;
    
    	struct gpio_desc *reset_gpio;
    	struct gpio_desc *lp_gpio;
    	struct gpio_desc *ac_detect_gpio;
    	struct gpio_desc *ce_gpio;
    
    	char model_name[I2C_NAME_SIZE];
    	int device_id;
    	bool mains_online;
    
    	struct bq2515x_init_data init_data;
    };
    
    static struct reg_default bq25150_reg_defs[] = {
    	{BQ2515X_FLAG0, 0x0},
    	{BQ2515X_FLAG1, 0x0},
    	{BQ2515X_FLAG2, 0x0},
    	{BQ2515X_FLAG3, 0x0},
    	{BQ2515X_MASK0, 0x0},
    	{BQ2515X_MASK1, 0x0},
    	{BQ2515X_MASK2, 0x71},
    	{BQ2515X_MASK3, 0x0},
    	{BQ2515X_VBAT_CTRL, 0x3C},
    	{BQ2515X_ICHG_CTRL, 0x8},
    	{BQ2515X_PCHRGCTRL, 0x2},
    	{BQ2515X_TERMCTRL, 0x14},
    	{BQ2515X_BUVLO, 0x0},
    	{BQ2515X_CHARGERCTRL0, 0x82},
    	{BQ2515X_CHARGERCTRL1, 0x42},
    	{BQ2515X_ILIMCTRL, 0x1},
    	{BQ2515X_LDOCTRL, 0xB0},
    	{BQ2515X_MRCTRL, 0x2A},
    	{BQ2515X_ICCTRL0, 0x10},
    	{BQ2515X_ICCTRL1, 0x0},
    	{BQ2515X_ICCTRL2, 0x0},
    	{BQ2515X_ADCCTRL0, 0x2},
    	{BQ2515X_ADCCTRL1, 0x40},
    	{BQ2515X_ADC_COMP1_M, 0x23},
    	{BQ2515X_ADC_COMP1_L, 0x20},
    	{BQ2515X_ADC_COMP2_M, 0x38},
    	{BQ2515X_ADC_COMP2_L, 0x90},
    	{BQ2515X_ADC_COMP3_M, 0x0},
    	{BQ2515X_ADC_COMP3_L, 0x0},
    	{BQ2515X_ADC_READ_EN, 0x0},
    	{BQ2515X_TS_FASTCHGCTRL, 0x34},
    	{BQ2515X_TS_COLD, 0x7C},
    	{BQ2515X_TS_COOL, 0x6D},
    	{BQ2515X_TS_WARM, 0x38},
    	{BQ2515X_TS_HOT, 0x27},
    	{BQ2515X_DEVICE_ID, 0x20},
    };
    
    static struct reg_default bq25155_reg_defs[] = {
    	{BQ2515X_FLAG0, 0x0},
    	{BQ2515X_FLAG1, 0x0},
    	{BQ2515X_FLAG2, 0x0},
    	{BQ2515X_FLAG3, 0x0},
    	{BQ2515X_MASK0, 0x0},
    	{BQ2515X_MASK1, 0x0},
    	{BQ2515X_MASK2, 0x71},
    	{BQ2515X_MASK3, 0x0},
    	{BQ2515X_VBAT_CTRL, 0x3C},
    	{BQ2515X_ICHG_CTRL, 0x8},
    	{BQ2515X_PCHRGCTRL, 0x2},
    	{BQ2515X_TERMCTRL, 0x14},
    	{BQ2515X_BUVLO, 0x0},
    	{BQ2515X_CHARGERCTRL0, 0x82},
    	{BQ2515X_CHARGERCTRL1, 0xC2},
    	{BQ2515X_ILIMCTRL, 0x6},
    	{BQ2515X_LDOCTRL, 0xB0},
    	{BQ2515X_MRCTRL, 0x2A},
    	{BQ2515X_ICCTRL0, 0x10},
    	{BQ2515X_ICCTRL1, 0x0},
    	{BQ2515X_ICCTRL2, 0x40},
    	{BQ2515X_ADCCTRL0, 0x2},
    	{BQ2515X_ADCCTRL1, 0x40},
    	{BQ2515X_ADC_COMP1_M, 0x23},
    	{BQ2515X_ADC_COMP1_L, 0x20},
    	{BQ2515X_ADC_COMP2_M, 0x38},
    	{BQ2515X_ADC_COMP2_L, 0x90},
    	{BQ2515X_ADC_COMP3_M, 0x0},
    	{BQ2515X_ADC_COMP3_L, 0x0},
    	{BQ2515X_ADC_READ_EN, 0x0},
    	{BQ2515X_TS_FASTCHGCTRL, 0x34},
    	{BQ2515X_TS_COLD, 0x7C},
    	{BQ2515X_TS_COOL, 0x6D},
    	{BQ2515X_TS_WARM, 0x38},
    	{BQ2515X_TS_HOT, 0x27},
    	{BQ2515X_DEVICE_ID, 0x35},
    };
    
    static struct reg_default bq21061_reg_defs[] = {
    	{BQ2515X_FLAG0, 0x0},
    	{BQ2515X_FLAG1, 0x0},
    	{BQ2515X_FLAG2, 0x0},
    	{BQ2515X_FLAG3, 0x0},
    	{BQ2515X_MASK0, 0x0},
    	{BQ2515X_MASK1, 0x0},
    	{BQ2515X_MASK2, 0x71},
    	{BQ2515X_MASK3, 0x0},
    	{BQ2515X_VBAT_CTRL, 0x3C},
    	{BQ2515X_ICHG_CTRL, 0x8},
    	{BQ2515X_PCHRGCTRL, 0x2},
    	{BQ2515X_TERMCTRL, 0x14},
    	{BQ2515X_BUVLO, 0x0},
    	{BQ2515X_CHARGERCTRL0, 0x82},
    	{BQ2515X_CHARGERCTRL1, 0xC2},
    	{BQ2515X_ILIMCTRL, 0x6},
    	{BQ2515X_LDOCTRL, 0xB0},
    	{BQ2515X_MRCTRL, 0x2A},
    	{BQ2515X_ICCTRL0, 0x10},
    	{BQ2515X_ICCTRL1, 0x0},
    	{BQ2515X_ICCTRL2, 0x40},
    	{BQ2515X_TS_FASTCHGCTRL, 0x34},
    	{BQ2515X_TS_COLD, 0x7C},
    	{BQ2515X_TS_COOL, 0x6D},
    	{BQ2515X_TS_WARM, 0x38},
    	{BQ2515X_TS_HOT, 0x27},
    	{BQ2515X_DEVICE_ID, 0x3A},
    };
    
    static bool bq2515x_is_ps_online(struct bq2515x_device *bq2515x)
    {
    	return bq2515x->mains_online;
    }
    
    static int bq2515x_wake_up(struct bq2515x_device *bq2515x)
    {
    	int ret;
    	int val;
    
    	/* Read the STAT register if we can read it then the device is out
    	 * of ship mode.  If the register cannot be read then attempt to wake
    	 * it up and enable the ADC.
    	 */
    	ret = regmap_read(bq2515x->regmap, BQ2515X_STAT0, &val);
    	if (!ret)
    		return ret;
    
    	/* Need to toggle LP and bring device out of ship mode. The device
    	 * will exit the ship mode when the MR pin is held low for at least
    	 * t_WAKE2 as shown in section 8.3.7.1 of the datasheet.
    	 */
    	if (bq2515x->lp_gpio)
    		gpiod_set_value_cansleep(bq2515x->lp_gpio, 0);
    
    	if (bq2515x->lp_gpio) {
    		gpiod_set_value_cansleep(bq2515x->reset_gpio, 0);
    		usleep_range(BQ2515X_TWAKE2_MIN_US, BQ2515X_TWAKE2_MAX_US);
    		gpiod_set_value_cansleep(bq2515x->reset_gpio, 1);
    	}
    
    	return regmap_write(bq2515x->regmap, BQ2515X_ADC_READ_EN, BIT(3));
    }
    
    static int bq2515x_update_ps_status(struct bq2515x_device *bq2515x)
    {
    	bool dc = false;
    	unsigned int val;
    	int ret;
    
    	if (bq2515x->ac_detect_gpio)
    		val = gpiod_get_value_cansleep(bq2515x->ac_detect_gpio);
    
    	else {
    		ret = regmap_read(bq2515x->regmap, BQ2515X_STAT0, &val);
    		if (ret < 0)
    			return ret;
    	}
    
    	dc = val & BQ2515X_VIN_GOOD;
    
    	ret = bq2515x->mains_online != dc;
    
    	bq2515x->mains_online = dc;
    
    	return ret;
    }
    
    static int bq2515x_disable_watchdog_timers(struct bq2515x_device *bq2515x)
    {
    	int ret;
    
    	ret = regmap_update_bits(bq2515x->regmap, BQ2515X_CHARGERCTRL0,
    			BQ2515X_WATCHDOG_DISABLE, BQ2515X_WATCHDOG_DISABLE);
    	if (ret < 0)
    		return ret;
    
    	return regmap_update_bits(bq2515x->regmap, BQ2515X_ICCTRL2,
    						BQ2515X_HWRESET_14S_WD, 0);
    }
    
    static int bq2515x_get_battery_voltage_now(struct bq2515x_device *bq2515x)
    {
    	int ret;
    	int vbat_msb;
    	int vbat_lsb;
    	uint32_t vbat_measurement;
    
    	if (!bq2515x_is_ps_online(bq2515x))
    		bq2515x_wake_up(bq2515x);
    
    	ret = regmap_read(bq2515x->regmap, BQ2515X_ADC_VBAT_M, &vbat_msb);
    	if (ret)
    		return ret;
    
    	ret = regmap_read(bq2515x->regmap, BQ2515X_ADC_VBAT_L, &vbat_lsb);
    	if (ret)
    		return ret;
    
    	vbat_measurement = (vbat_msb << 8) | vbat_lsb;
    
    	return vbat_measurement * (BQ2515X_UV_FACTOR / BQ2515X_DIVISOR) * 6;
    }
    
    static int bq2515x_get_battery_current_now(struct bq2515x_device *bq2515x)
    {
    	int ret;
    	int ichg_msb;
    	int ichg_lsb;
    	uint32_t ichg_measurement;
    	u16 ichg_multiplier = BQ2515X_ICHG_RNG_1B0_UA;
    	unsigned int ichg_reg_code, reg_code;
    	unsigned int icharge_range = 0, pchrgctrl;
    	unsigned int buvlo, vlowv_sel, vlowv = BQ2515X_VLOWV_SEL_1B0_UV;
    
    	if (!bq2515x_is_ps_online(bq2515x))
    		return -ENODATA;
    
    	ret = regmap_read(bq2515x->regmap, BQ2515X_ADC_ICHG_M, &ichg_msb);
    	if (ret < 0)
    		return ret;
    
    	ret = regmap_read(bq2515x->regmap, BQ2515X_ADC_ICHG_L, &ichg_lsb);
    	if (ret < 0)
    		return ret;
    
    	ichg_measurement = (ichg_msb << 8) | ichg_lsb;
    
    	ret = regmap_read(bq2515x->regmap, BQ2515X_BUVLO, &buvlo);
    	if (ret < 0)
    		return ret;
    
    	vlowv_sel = buvlo & BQ2515X_VLOWV_SEL;
    
    	if (vlowv_sel)
    		vlowv = BQ2515X_VLOWV_SEL_1B1_UV;
    
    	if (bq2515x_get_battery_voltage_now(bq2515x) < vlowv) {
    		ret = regmap_read(bq2515x->regmap, BQ2515X_PCHRGCTRL,
    								&pchrgctrl);
    		if (ret < 0)
    			return ret;
    		reg_code = pchrgctrl & BQ2515X_PRECHARGE_MASK;
    	} else {
    		ret = regmap_read(bq2515x->regmap, BQ2515X_ICHG_CTRL,
    							&ichg_reg_code);
    		if (ret < 0)
    			return ret;
    		reg_code = ichg_reg_code;
    	}
    
    	ret = regmap_read(bq2515x->regmap, BQ2515X_PCHRGCTRL, &pchrgctrl);
    	if (ret < 0)
    		return ret;
    
    	icharge_range = pchrgctrl & BQ2515X_ICHARGE_RANGE;
    
    	if (icharge_range)
    		ichg_multiplier = BQ2515X_ICHG_RNG_1B1_UA;
    
    	return reg_code * (ichg_multiplier * ichg_measurement
    						/ BQ2515X_ICHG_DIVISOR);
    }
    
    static bool bq2515x_get_charge_disable(struct bq2515x_device *bq2515x)
    {
    	int ret;
    	int ce_pin = 0;
    	int icctrl2;
    	int charger_disable;
    
    	if (bq2515x->ce_gpio)
    		ce_pin = gpiod_get_value_cansleep(bq2515x->ce_gpio);
    
    	ret = regmap_read(bq2515x->regmap, BQ2515X_ICCTRL2, &icctrl2);
    	if (ret < 0)
    		return ret;
    
    	charger_disable = icctrl2 & BQ2515X_CHARGER_DISABLE;
    
    	if (charger_disable || ce_pin)
    		return true;
    
    	return false;
    }
    
    static int bq2515x_set_charge_disable(struct bq2515x_device *bq2515x, int val)
    {
    	if (bq2515x->ce_gpio)
    		gpiod_set_value_cansleep(bq2515x->ce_gpio, val);
    
    	return regmap_update_bits(bq2515x->regmap, BQ2515X_ICCTRL2,
    					BQ2515X_CHARGER_DISABLE, val);
    }
    
    static int bq2515x_get_const_charge_current(struct bq2515x_device *bq2515x)
    {
    	int ret;
    	u16 ichg_multiplier = BQ2515X_ICHG_RNG_1B0_UA;
    	unsigned int ichg_reg_code;
    	unsigned int pchrgctrl;
    	unsigned int icharge_range;
    
    	ret = regmap_read(bq2515x->regmap, BQ2515X_ICHG_CTRL, &ichg_reg_code);
    	if (ret < 0)
    		return ret;
    
    	ret = regmap_read(bq2515x->regmap, BQ2515X_PCHRGCTRL, &pchrgctrl);
    	if (ret < 0)
    		return ret;
    
    	icharge_range = pchrgctrl & BQ2515X_ICHARGE_RANGE;
    
    	if (icharge_range)
    		ichg_multiplier = BQ2515X_ICHG_RNG_1B1_UA;
    
    	return ichg_reg_code * ichg_multiplier;
    }
    
    static int bq2515x_set_const_charge_current(struct bq2515x_device *bq2515x,
    								int val)
    {
    	int ret;
    	unsigned int ichg_reg_code;
    	u16 ichg_multiplier = BQ2515X_ICHG_RNG_1B0_UA;
    	unsigned int icharge_range = 0;
    
    	if (val > BQ2515X_ICHG_MAX_UA || val < BQ2515X_ICHG_MIN_UA)
    		return -EINVAL;
    
    	if (val > BQ2515X_ICHG_CURR_STEP_THRESH_UA) {
    		ichg_multiplier = BQ2515X_ICHG_RNG_1B1_UA;
    		icharge_range = BQ2515X_ICHARGE_RANGE;
    	}
    
    	bq2515x_set_charge_disable(bq2515x, 1);
    
    	ret = regmap_update_bits(bq2515x->regmap, BQ2515X_PCHRGCTRL,
    					BQ2515X_ICHARGE_RANGE, icharge_range);
    	if (ret < 0)
    		return ret;
    
    	ichg_reg_code = val / ichg_multiplier;
    
    	ret = regmap_write(bq2515x->regmap, BQ2515X_ICHG_CTRL, ichg_reg_code);
    	if (ret < 0)
    		return ret;
    
    	return bq2515x_set_charge_disable(bq2515x, 0);
    }
    
    static int bq2515x_get_precharge_current(struct bq2515x_device *bq2515x)
    {
    	int ret;
    	unsigned int pchrgctrl;
    	unsigned int icharge_range;
    	u16 precharge_multiplier = BQ2515X_ICHG_RNG_1B0_UA;
    	unsigned int precharge_reg_code;
    
    	ret = regmap_read(bq2515x->regmap, BQ2515X_PCHRGCTRL, &pchrgctrl);
    	if (ret < 0)
    		return ret;
    
    	icharge_range = pchrgctrl & BQ2515X_ICHARGE_RANGE;
    
    	if (icharge_range)
    		precharge_multiplier = BQ2515X_ICHG_RNG_1B1_UA;
    
    	precharge_reg_code = pchrgctrl & BQ2515X_PRECHARGE_MASK;
    
    	return precharge_reg_code * precharge_multiplier;
    }
    
    static int bq2515x_set_precharge_current(struct bq2515x_device *bq2515x,
    					int val)
    {
    	int ret;
    	unsigned int pchrgctrl;
    	unsigned int icharge_range;
    	unsigned int precharge_reg_code;
    	u16 precharge_multiplier = BQ2515X_ICHG_RNG_1B0_UA;
    	u16 precharge_max_ua = BQ2515X_PRECHRG_ICHRG_RNGE_1875_UA;
    
    	ret = regmap_read(bq2515x->regmap, BQ2515X_PCHRGCTRL, &pchrgctrl);
    	if (ret < 0)
    		return ret;
    
    	icharge_range = pchrgctrl & BQ2515X_ICHARGE_RANGE;
    
    	if (icharge_range) {
    		precharge_max_ua = BQ2515X_PRECHRG_ICHRG_RNGE_3750_UA;
    		precharge_multiplier = BQ2515X_ICHG_RNG_1B1_UA;
    	}
    	if (val > precharge_max_ua || val < BQ2515X_ICHG_MIN_UA)
    		return -EINVAL;
    
    	precharge_reg_code = val / precharge_multiplier;
    
    	ret = bq2515x_set_charge_disable(bq2515x, 1);
    	if (ret < 0)
    		return ret;
    
    	ret = regmap_update_bits(bq2515x->regmap, BQ2515X_PCHRGCTRL,
    				BQ2515X_PRECHARGE_MASK, precharge_reg_code);
    	if (ret < 0)
    		return ret;
    
    	return bq2515x_set_charge_disable(bq2515x, 0);
    }
    
    static int bq2515x_charging_status(struct bq2515x_device *bq2515x,
    				   union power_supply_propval *val)
    {
    	bool status0_no_fault;
    	bool status1_no_fault;
    	bool ce_status;
    	bool charge_done;
    	unsigned int status;
    	int ret;
    
    	if (!bq2515x_is_ps_online(bq2515x)) {
    		val->intval = POWER_SUPPLY_STATUS_DISCHARGING;
    		return 0;
    	}
    
    	ret = regmap_read(bq2515x->regmap, BQ2515X_STAT0, &status);
    	if (ret)
    		return ret;
    
    	/**
    	 * The code block below is used to determine if any faults from the
    	 * STAT0 register are disbaling charging or if the charge has completed
    	 * according to the CHARGE_DONE_STAT bit.
    	 */
    	if (((status & BQ2515X_STAT0_MASK) == true) &
    			((status & BQ2515X_CHRG_DONE) == false)) {
    		status0_no_fault = true;
    		charge_done = false;
    	} else if (status & BQ2515X_CHRG_DONE) {
    		charge_done = true;
    		status0_no_fault = false;
    	} else {
    		status0_no_fault = false;
    		charge_done = false;
    	}
    
    	ret = regmap_read(bq2515x->regmap, BQ2515X_STAT1, &status);
    	if (ret)
    		return ret;
    	/**
    	 *The code block below is used to determine if any faults from the
    	 * STAT1 register are disbaling charging
    	 */
    	if ((status & BQ2515X_STAT1_MASK) == false)
    		status1_no_fault = true;
    	else
    		status1_no_fault = false;
    
    	ce_status = (!bq2515x_get_charge_disable(bq2515x));
    
    	/**
    	 *If there are no faults and charging is enabled, then status is
    	 *charging. Otherwise, if charging is complete, then status is full.
    	 *Otherwise, if a fault exists or charging is disbaled, then status is
    	 *not charging
    	 */
    	if (status0_no_fault & status1_no_fault & ce_status)
    		val->intval = POWER_SUPPLY_STATUS_CHARGING;
    	else if (charge_done)
    		val->intval = POWER_SUPPLY_STATUS_FULL;
    	else if (!(status0_no_fault & status1_no_fault & ce_status))
    		val->intval = POWER_SUPPLY_STATUS_NOT_CHARGING;
    
    	return ret;
    }
    
    static int bq2515x_get_batt_reg(struct bq2515x_device *bq2515x)
    {
    	int vbat_reg_code;
    	int ret;
    
    	ret = regmap_read(bq2515x->regmap, BQ2515X_VBAT_CTRL, &vbat_reg_code);
    	if (ret)
    		return ret;
    
    	return BQ2515X_VBAT_BASE_VOLT + vbat_reg_code * BQ2515X_VBAT_STEP_UV;
    }
    
    static int bq2515x_set_batt_reg(struct bq2515x_device *bq2515x, int val)
    {
    	int vbat_reg_code;
    
    	if (val > BQ2515X_VBAT_REG_MAX || val < BQ2515X_VBAT_REG_MIN)
    		return -EINVAL;
    
    	vbat_reg_code = (val - BQ2515X_VBAT_BASE_VOLT) / BQ2515X_VBAT_STEP_UV;
    
    	return regmap_write(bq2515x->regmap, BQ2515X_VBAT_CTRL, vbat_reg_code);
    }
    
    static int bq2515x_get_ilim_lvl(struct bq2515x_device *bq2515x)
    {
    	int ret;
    	int ilimctrl;
    
    	ret = regmap_read(bq2515x->regmap, BQ2515X_ILIMCTRL, &ilimctrl);
    	if (ret)
    		return ret;
    
    	return bq2515x_ilim_lvl_values[ilimctrl & BQ2515X_ILIM_MASK];
    }
    
    static int bq2515x_set_ilim_lvl(struct bq2515x_device *bq2515x, int val)
    {
    	int i;
    
    	for (i = 0; i < ARRAY_SIZE(bq2515x_ilim_lvl_values); i++) {
    		if (val == bq2515x_ilim_lvl_values[i])
    			break;
    
    		if (val > bq2515x_ilim_lvl_values[i - 1] &&
    		    val < bq2515x_ilim_lvl_values[i]) {
    			if (val - bq2515x_ilim_lvl_values[i - 1] <
    			    bq2515x_ilim_lvl_values[i] - val) {
    				i = i - 1;
    				break;
    			}
    		}
    	}
    
    	return regmap_write(bq2515x->regmap, BQ2515X_ILIMCTRL, i);
    }
    
    static int bq2515x_power_supply_property_is_writeable(struct power_supply *psy,
    					enum power_supply_property prop)
    {
    	switch (prop) {
    	case POWER_SUPPLY_PROP_INPUT_CURRENT_LIMIT:
    	case POWER_SUPPLY_PROP_CONSTANT_CHARGE_VOLTAGE:
    	case POWER_SUPPLY_PROP_CONSTANT_CHARGE_CURRENT:
    	case POWER_SUPPLY_PROP_PRECHARGE_CURRENT:
    		return true;
    	default:
    		return false;
    	}
    }
    
    static int bq2515x_charger_get_health(struct bq2515x_device *bq2515x,
    				      union power_supply_propval *val)
    {
    	int health = POWER_SUPPLY_HEALTH_GOOD;
    	int ret;
    	unsigned int stat1;
    	unsigned int flag3;
    
    	if (!bq2515x_is_ps_online(bq2515x))
    		bq2515x_wake_up(bq2515x);
    
    	ret = regmap_read(bq2515x->regmap, BQ2515X_FLAG3, &flag3);
    	if (ret)
    		return ret;
    
    	if (flag3 & BQ2515X_SAFETY_TIMER_EXP) {
    		health = POWER_SUPPLY_HEALTH_SAFETY_TIMER_EXPIRE;
    		goto ret_health;
    	}
    
    	if (stat1 & BQ2515X_VIN_OVP_FAULT_STAT) {
    		health = POWER_SUPPLY_HEALTH_OVERVOLTAGE;
    		goto ret_health;
    	}
    
    	ret = regmap_read(bq2515x->regmap, BQ2515X_STAT1, &stat1);
    	if (ret)
    		return ret;
    
    	if (stat1 & BQ2515X_HEALTH_MASK) {
    		switch (stat1 & BQ2515X_HEALTH_MASK) {
    		case BQ2515X_TS_HOT_STAT:
    			health = POWER_SUPPLY_HEALTH_HOT;
    			break;
    		case BQ2515X_TS_WARM_STAT:
    			health = POWER_SUPPLY_HEALTH_WARM;
    			break;
    		case BQ2515X_TS_COOL_STAT:
    			health = POWER_SUPPLY_HEALTH_COOL;
    			break;
    		case BQ2515X_TS_COLD_STAT:
    			health = POWER_SUPPLY_HEALTH_COLD;
    			break;
    		default:
    			health = POWER_SUPPLY_HEALTH_UNKNOWN;
    			break;
    		}
    	}
    	
    	goto ret_health;
    
    ret_health:
    	val->intval = health;
    	return 0;
    }
    
    static int bq2515x_mains_set_property(struct power_supply *psy,
    		enum power_supply_property prop,
    		const union power_supply_propval *val)
    {
    	struct bq2515x_device *bq2515x = power_supply_get_drvdata(psy);
    	int ret;
    
    	switch (prop) {
    	case POWER_SUPPLY_PROP_INPUT_CURRENT_LIMIT:
    		ret = bq2515x_set_ilim_lvl(bq2515x, val->intval);
    		break;
    	case POWER_SUPPLY_PROP_CONSTANT_CHARGE_VOLTAGE:
    		ret = bq2515x_set_batt_reg(bq2515x, val->intval);
    		break;
    	case POWER_SUPPLY_PROP_CONSTANT_CHARGE_CURRENT:
    		ret = bq2515x_set_const_charge_current(bq2515x, val->intval);
    		break;
    	case POWER_SUPPLY_PROP_PRECHARGE_CURRENT:
    		ret = bq2515x_set_precharge_current(bq2515x, val->intval);
    		break;
    	default:
    		return -EINVAL;
    	}
    
    	return ret;
    }
    
    static int bq2515x_mains_get_property(struct power_supply *psy,
    				     enum power_supply_property prop,
    				     union power_supply_propval *val)
    {
    	struct bq2515x_device *bq2515x = power_supply_get_drvdata(psy);
    	int ret = 0;
    
    	switch (prop) {
    	case POWER_SUPPLY_PROP_ONLINE:
    		val->intval = bq2515x->mains_online;
    		break;
    	case POWER_SUPPLY_PROP_CONSTANT_CHARGE_CURRENT:
    		ret = bq2515x_get_const_charge_current(bq2515x);
    		if (ret < 0)
    			return ret;
    
    		val->intval = ret;
    		break;
    	case POWER_SUPPLY_PROP_PRECHARGE_CURRENT:
    		ret = bq2515x_get_precharge_current(bq2515x);
    		if (ret < 0)
    			return ret;
    
    		val->intval = ret;
    		break;
    	case POWER_SUPPLY_PROP_INPUT_CURRENT_LIMIT:
    		ret = bq2515x_get_ilim_lvl(bq2515x);
    		if (ret < 0)
    			return ret;
    
    		val->intval = ret;
    		break;
    	case POWER_SUPPLY_PROP_CONSTANT_CHARGE_VOLTAGE:
    		ret = bq2515x_get_batt_reg(bq2515x);
    		if (ret < 0)
    			return ret;
    
    		val->intval = ret;
    		break;
    	case POWER_SUPPLY_PROP_MODEL_NAME:
    		val->strval = bq2515x->model_name;
    		break;
    	case POWER_SUPPLY_PROP_MANUFACTURER:
    		val->strval = BQ2515X_MANUFACTURER;
    		break;
    	case POWER_SUPPLY_PROP_VOLTAGE_MAX:
    		val->intval = BQ2515X_VBAT_REG_MAX;
    		break;
    	case POWER_SUPPLY_PROP_VOLTAGE_MIN:
    		val->intval = BQ2515X_VBAT_REG_MIN;
    		break;
    	case POWER_SUPPLY_PROP_CONSTANT_CHARGE_CURRENT_MAX:
    		val->intval = BQ2515X_ICHG_MAX_UA;
    		break;
    	default:
    		return -EINVAL;
    	}
    
    	return ret;
    }
    
    static int bq2515x_battery_get_property(struct power_supply *psy,
    				       enum power_supply_property prop,
    				       union power_supply_propval *val)
    {
    	struct bq2515x_device *bq2515x = power_supply_get_drvdata(psy);
    	int ret;
    
    	ret = bq2515x_update_ps_status(bq2515x);
    	if (ret < 0)
    		return ret;
    
    	switch (prop) {
    
    	case POWER_SUPPLY_PROP_STATUS:
    		if (!bq2515x_is_ps_online(bq2515x)) {
    			val->intval = POWER_SUPPLY_STATUS_DISCHARGING;
    			break;
    		}
    
    		ret = bq2515x_charging_status(bq2515x, val);
    		break;
    	case POWER_SUPPLY_PROP_VOLTAGE_NOW:
    		ret = bq2515x_get_battery_voltage_now(bq2515x);
    		if (ret < 0)
    			return ret;
    
    		val->intval = ret;
    		break;
    	case POWER_SUPPLY_PROP_CURRENT_NOW:
    		ret = bq2515x_get_battery_current_now(bq2515x);
    		if (ret < 0)
    			return ret;
    
    		val->intval = ret;
    		break;
    	case POWER_SUPPLY_PROP_HEALTH:
    		ret = bq2515x_charger_get_health(bq2515x, val);
    		if (ret)
    			val->intval = POWER_SUPPLY_HEALTH_UNKNOWN;
    		break;
    	default:
    		return -EINVAL;
    	}
    	return 0;
    }
    
    static enum power_supply_property bq2515x_battery_properties[] = {
    	POWER_SUPPLY_PROP_STATUS,
    	POWER_SUPPLY_PROP_HEALTH,
    	POWER_SUPPLY_PROP_VOLTAGE_NOW,
    	POWER_SUPPLY_PROP_CURRENT_NOW,
    };
    
    static enum power_supply_property bq21061_battery_properties[] = {
    	POWER_SUPPLY_PROP_STATUS,
    	POWER_SUPPLY_PROP_HEALTH,
    };
    
    static enum power_supply_property bq2515x_charger_properties[] = {
    	POWER_SUPPLY_PROP_ONLINE,
    	POWER_SUPPLY_PROP_CONSTANT_CHARGE_CURRENT,
    	POWER_SUPPLY_PROP_PRECHARGE_CURRENT,
    	POWER_SUPPLY_PROP_CONSTANT_CHARGE_VOLTAGE,
    	POWER_SUPPLY_PROP_INPUT_CURRENT_LIMIT,
    	POWER_SUPPLY_PROP_VOLTAGE_MAX,
    	POWER_SUPPLY_PROP_VOLTAGE_MIN,
    	POWER_SUPPLY_PROP_MODEL_NAME,
    	POWER_SUPPLY_PROP_MANUFACTURER,
    };
    
    static struct power_supply_desc bq2515x_mains_desc = {
    	.name			= "bq2515x-mains",
    	.type			= POWER_SUPPLY_TYPE_MAINS,
    	.get_property		= bq2515x_mains_get_property,
    	.set_property		= bq2515x_mains_set_property,
    	.properties		= bq2515x_charger_properties,
    	.num_properties		= ARRAY_SIZE(bq2515x_charger_properties),
    	.property_is_writeable = bq2515x_power_supply_property_is_writeable,
    
    };
    
    static struct power_supply_desc bq2515x_battery_desc = {
    	.name			= "bq2515x-battery",
    	.type			= POWER_SUPPLY_TYPE_BATTERY,
    	.get_property		= bq2515x_battery_get_property,
    	.properties		= bq2515x_battery_properties,
    	.num_properties		= ARRAY_SIZE(bq2515x_battery_properties),
    };
    
    static struct power_supply_desc bq21061_battery_desc = {
    	.name			= "bq2515x-battery",
    	.type			= POWER_SUPPLY_TYPE_BATTERY,
    	.get_property		= bq2515x_battery_get_property,
    	.properties		= bq21061_battery_properties,
    	.num_properties		= ARRAY_SIZE(bq21061_battery_properties),
    };
    
    static int bq2515x_power_supply_register(struct bq2515x_device *bq2515x)
    {
    	struct power_supply_config psy_cfg = { .drv_data = bq2515x, };
    
    	bq2515x->mains = devm_power_supply_register(bq2515x->dev,
    						    &bq2515x_mains_desc,
    						    &psy_cfg);
    	if (IS_ERR(bq2515x->mains))
    		return -EINVAL;
    	
    	switch (bq2515x->device_id) {
    	case BQ25150:
    	case BQ25155:
    	bq2515x->battery = devm_power_supply_register(bq2515x->dev,
    						      &bq2515x_battery_desc,
    						      &psy_cfg);
    	break;
    	case BQ21061:
    	bq2515x->battery = devm_power_supply_register(bq2515x->dev,
    						      &bq21061_battery_desc,
    						      &psy_cfg);
    	break;
    	}
    
    	if (IS_ERR(bq2515x->battery))
    		return -EINVAL;
    
    	return 0;
    }
    
    static int bq2515x_hw_init(struct bq2515x_device *bq2515x)
    {
    	int ret = 0;
    
    	if (bq2515x->init_data.ichg)
    		ret = bq2515x_set_const_charge_current(bq2515x,
    						bq2515x->init_data.ichg);
    
    	if (ret)
    		goto err_out;
    
    	if (bq2515x->init_data.ilim)
    		ret = bq2515x_set_ilim_lvl(bq2515x, bq2515x->init_data.ilim);
    
    	if (ret)
    		goto err_out;
    
    	if (bq2515x->init_data.vreg)
    		ret = bq2515x_set_batt_reg(bq2515x, bq2515x->init_data.vreg);
    
    	if (ret)
    		goto err_out;
    
    	ret = bq2515x_disable_watchdog_timers(bq2515x);
    
    	if (ret)
    		goto err_out;
    
    err_out:
    	return ret;
    }
    
    static int bq2515x_read_properties(struct bq2515x_device *bq2515x)
    {
    	int ret;
    
    	ret = device_property_read_u32(bq2515x->dev,
    				      "constant-charge-current-max-microamp",
    				      &bq2515x->init_data.ichg);
    	if (ret)
    		bq2515x->init_data.ichg = BQ2515X_DEFAULT_ICHG_UA;
    
    	ret = device_property_read_u32(bq2515x->dev,
    				      "precharge-current-max-microamp",
    				      &bq2515x->init_data.iprecharge);
    	if (ret)
    		bq2515x->init_data.iprecharge = BQ2515X_DEFAULT_IPRECHARGE_UA;
    
    	ret = device_property_read_u32(bq2515x->dev,
    				      "input-current-limit-microamp",
    				      &bq2515x->init_data.ilim);
    	if (ret)
    		switch (bq2515x->device_id) {
    		case BQ25150:
    			bq2515x->init_data.ilim = BQ25150_DEFAULT_ILIM_UA;
    			break;
    		case BQ25155:
    		case BQ21061:
    			bq2515x->init_data.ilim = BQ25155_DEFAULT_ILIM_UA;
    			break;
    		}
    
    	ret = device_property_read_u32(bq2515x->dev,
    				      "constant-charge-voltage-max-microvolt",
    				      &bq2515x->init_data.vreg);
    	if (ret)
    		bq2515x->init_data.vreg = BQ2515X_DEFAULT_VBAT_REG_UV;
    
    	bq2515x->ac_detect_gpio = devm_gpiod_get_optional(bq2515x->dev,
    						   "ac_detect", GPIOD_IN);
    	if (IS_ERR(bq2515x->ac_detect_gpio))
    		dev_info(bq2515x->dev, "ac_detect GPIO not defined");
    
    	bq2515x->reset_gpio = devm_gpiod_get_optional(bq2515x->dev,
    						   "reset", GPIOD_OUT_LOW);
    	if (IS_ERR(bq2515x->reset_gpio)) {
    		if (PTR_ERR(bq2515x->reset_gpio) == -EPROBE_DEFER)
    			return -EPROBE_DEFER;
    	}
    
    	bq2515x->lp_gpio = devm_gpiod_get_optional(bq2515x->dev, "low-power",
    						   GPIOD_OUT_LOW);
    	if (IS_ERR(bq2515x->lp_gpio)) {
    		if (PTR_ERR(bq2515x->lp_gpio) == -EPROBE_DEFER)
    			return -EPROBE_DEFER;
    	}
    
    	bq2515x->ce_gpio = devm_gpiod_get_optional(bq2515x->dev,
    						   "charge-enable",
    						   GPIOD_OUT_LOW);
    	if (IS_ERR(bq2515x->ce_gpio)) {
    		if (PTR_ERR(bq2515x->ce_gpio) == -EPROBE_DEFER)
    			return -EPROBE_DEFER;
    	}
    
    	return 0;
    }
    
    static bool bq2515x_volatile_register(struct device *dev, unsigned int reg)
    {
    	switch (reg) {
    	case BQ2515X_STAT0 ... BQ2515X_FLAG3:
    	case BQ2515X_ADC_VBAT_M ... BQ2515X_ADC_IIN_L:
    		return true;
    	default:
    		return false;
    	}
    }
    
    static const struct regmap_config bq25150_regmap_config = {
    	.reg_bits = 8,
    	.val_bits = 8,
    
    	.max_register		= BQ2515X_DEVICE_ID,
    	.reg_defaults		= bq25150_reg_defs,
    	.num_reg_defaults	= ARRAY_SIZE(bq25150_reg_defs),
    	.cache_type		= REGCACHE_RBTREE,
    	.volatile_reg		= bq2515x_volatile_register,
    };
    
    static const struct regmap_config bq25155_regmap_config = {
    	.reg_bits = 8,
    	.val_bits = 8,
    
    	.max_register		= BQ2515X_DEVICE_ID,
    	.reg_defaults		= bq25155_reg_defs,
    	.num_reg_defaults	= ARRAY_SIZE(bq25155_reg_defs),
    	.cache_type		= REGCACHE_RBTREE,
    	.volatile_reg		= bq2515x_volatile_register,
    };
    
    static const struct regmap_config bq21061_regmap_config = {
    	.reg_bits = 8,
    	.val_bits = 8,
    
    	.max_register		= BQ2515X_DEVICE_ID,
    	.reg_defaults		= bq21061_reg_defs,
    	.num_reg_defaults	= ARRAY_SIZE(bq21061_reg_defs),
    	.cache_type		= REGCACHE_RBTREE,
    	.volatile_reg		= bq2515x_volatile_register,
    };
    
    static int bq2515x_probe(struct i2c_client *client,
    			 const struct i2c_device_id *id)
    {
    	struct device *dev = &client->dev;
    	struct bq2515x_device *bq;
    	int ret;
    
    	bq = devm_kzalloc(dev, sizeof(*bq), GFP_KERNEL);
    	if (!bq)
    		return -ENOMEM;
    
    	bq->client = client;
    	bq->dev = dev;
    
    	mutex_init(&bq->lock);
    
    	strncpy(bq->model_name, id->name, I2C_NAME_SIZE);
    
    	bq->device_id = id->driver_data;
    
    	switch (bq->device_id) {
    	case BQ25150:
    		bq->regmap = devm_regmap_init_i2c(client,
    						&bq25150_regmap_config);
    		break;
    	case BQ25155:
    		bq->regmap = devm_regmap_init_i2c(client,
    						&bq25155_regmap_config);
    		break;
    	case BQ21061:
    		bq->regmap = devm_regmap_init_i2c(client,
    						&bq21061_regmap_config);
    		break;
    	}
    
    	if (IS_ERR(bq->regmap)) {
    		dev_err(dev, "failed to allocate register map\n");
    		return PTR_ERR(bq->regmap);
    	}
    
    	i2c_set_clientdata(client, bq);
    
    	ret = bq2515x_read_properties(bq);
    	if (ret) {
    		dev_err(dev, "Failed to read device tree properties %d\n",
    									ret);
    		goto err_out;
    	}
    
    	ret = bq2515x_hw_init(bq);
    	if (ret) {
    		dev_err(dev, "Cannot initialize the chip.\n");
    		goto err_out;
    	}
    
    	return bq2515x_power_supply_register(bq);
    
    err_out:
    	mutex_destroy(&bq->lock);
    	return ret;
    }
    
    static const struct i2c_device_id bq2515x_i2c_ids[] = {
    	{ "bq25150", BQ25150, },
    	{ "bq25155", BQ25155, },
    	{ "bq21061", BQ21061, },
    	{},
    };
    MODULE_DEVICE_TABLE(i2c, bq2515x_i2c_ids);
    
    static const struct of_device_id bq2515x_of_match[] = {
    	{ .compatible = "ti,bq25150", },
    	{ .compatible = "ti,bq25155", },
    	{ .compatible = "ti,bq21061", },
    	{ },
    };
    MODULE_DEVICE_TABLE(of, bq2515x_of_match);
    
    static struct i2c_driver bq2515x_driver = {
    	.driver = {
    		.name = "bq2515x-charger",
    		.of_match_table = bq2515x_of_match,
    	},
    	.probe = bq2515x_probe,
    	.id_table = bq2515x_i2c_ids,
    };
    module_i2c_driver(bq2515x_driver);
    
    MODULE_AUTHOR("Dan Murphy <dmurphy@ti.com>");
    MODULE_AUTHOR("Ricardo Rivera-Matos <r-rivera-matos@ti.com>");
    MODULE_DESCRIPTION("BQ2515X charger driver");
    MODULE_LICENSE("GPL v2");
    
    

  • thanks for the driver. Could you also provide the header file?

  • Hello,

    The header file for linux should be publicly available.