This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5108: can Pin2(NC) be connected to VDD or GND?

Part Number: LM5108

Hi,

LM5108 pin 2 is NC.

can Pin2(NC) be connected to VDD or GND?

thanks.

  • Hi, Max,

    Ni hao!!!

    Yes, for the LM5108, NC means No internal connection, so it is truly floating. So you can connected it to either the thermal pad (ground) or the VDD pin "next door."

    If this answered your question, please press the Green button, Max.