Other Parts Discussed in Thread: BQ76930, BQSTUDIO, BQ78350-R1
Hi,
I have an 8 cell (8S) LiFePO4 battery pack assembled and wired up to the EVM. Power for the board is supplied by -ve from cell 1 and +ve from cell 8, i.e. Vcc is around 26-27V (because the cells are not fully charged).
I have a DC power supply set at 29.2V and 500mA (which is the charging voltage for 8 cells) and I would like to connect this to the battery so that I can observe the EVM doing its cell balancing and over-charge functions. However when I connect the power supply to the Batt- and Batt+ terminals of the board, I notice that the voltage for Cells 1 and 8 rise above 4V which is getting very close to their max of 4.2V - the remaining cells are all at a much lower value. I've attached a picture of the register readings which shows this odd imbalance.
Just wondering if I've connected the power supply (the charger) correctly for this exercise or is there some other reason why just these 2 cells should be reading so high?
Cheers,