Hello,
I have a 15pF capacitive load that I need to drive with a 15-cycle pulse train. I'd like to use a half-bridge where the high rail is 15V and the negative rail is -15V. (One end of my capacitive load is required to stay grounded). My system will run from a single Li-poly battery so I will have switching converters to generate the +-15V rail supplies. However, my microcontroller that will generate the control signals for driving the half-bridge will run from 0V to 3V. I was wondering if anyone might have any suggestions for the most efficient way to do the level translations for driving the half-bridge? That is, I'm looking for overall system efficiency. For instance, I'd like to get the +-15V switching converters to start up as quickly as possible and I'd like to turn them off as soon as I'm done driving the pulse train, and keep them off until I need to repeat this sequence. It would be good not to waste a lot of energy in the gate drivers. Any suggestions? Thank you.