hello,
IDPM_STAT of REG13 is described as IINDPM Status.
As shown in the following data sheet excerpt, the limiting current varies depending on the ICO_EN register setting.
Is IDPM_STAT set to 1 as follows?
When ICO_EN is 1, IDPM_STAT is 1 when the current is limited by IDPM_LIM.
When ICO_EN = 0, IDPM_STAT is 1 when the current is limited by IINLIM.
Data sheet excerpt
The actual input current limit used by the Dynamic Power Management is reported in IDPM_LIM register while Input Current Optimizer is enabled (ICO_EN = 1) or set by IINLIM register when the algorithm is disabled (ICO_EN = 0).
best regards