Other Parts Discussed in Thread: LM5026, LM5025
Hi,
I have a couple of question regarding the evaluation board and performance of the LM5026 controller:
1-) I tried to SYNC to an external frequency clock directly applying a pulsed signal (Sync pulse width > 15ns, Sync threshold: 1V-2V, higher freq than free running freq set by RT) through a resistor(to limit the current) directly to J3(SYNC1). This procedure does not work. I have done this into the LM5025 and works, is there any difference between these two controllers regarding the SYNC option?
Datasheet of LM5026 recommends an open drain output for the interface between LM5026 and the external clock, but is it mandatory for external SYNC? I would appreciate more info about how the Sync works in this controller.
1-)I would like to know the part number of the output capacitors(C19&C20) of the EVAL board, in the BOM, there is a part number for the ceramic caps(C21-C23: 68uF) and tantalum caps(C19&C20: 330uF), in the EVAL there are not tantalum caps, instead there are another set of ceramic(orange colored) what is the part number of the real C19 and C20?
Many thanks,