This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS610985: TPS610985 + SuperCAP

Part Number: TPS610985
Other Parts Discussed in Thread: TPS61098

Hi,

We are using TPS610985 in our device and 1F supercapacitor parallel to the boost converter TPS610985 as output capacitor in order to handle the high load for RF transmission. Our device main supply is primary battery alkaline which cannot handle the RF load transmission of NB-IoT module. So we added boost converter and supercap in our design to maximize the energy of the battery as well. 

Is there upper limit for the output capacitance value? Also, do you recommend to place the supercapacitor prior to boost converter or after, which is more efficient method?

Thank you.