This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS1663: OVLO: Over Voltage Trip Point Too Low

Part Number: TPS1663

Team - I am helping my customer verify their operating points before they design it in. We modified the EVM as indicated below and the resulting OV trip point is lower than calculated. What are we missing? Notes from the customer as follows:

I was able to get into the lab this morning to take a look at the TPS1663 development board.  I have made the following modifications to this board to mimic what is going to be present in the final design.  During the testing I observed that the OV trip point was not working as designed.  Below is the configuration of the development board:

 

Required Modifications

Ref. Des

Rockwell Part Number

Value

Tolerance

Voltage

Package Size

R2

LAB STOCK

330kΩ

1%

 

603

R3

PN-412491

82.5kΩ

1%

 

603

R4

LAB STOCK

10kΩ

1%

 

603

R5

PN-412489

34kΩ

1%

 

603

R6

PN-202416

5.76kΩ

1%

 

603

C4

21505-162-09

0.056ɥ

10%

25V

603

 

Min. Calculated Operating Points

Nom. Calculated Operating Points

Max. Calculated Operating Points

Under-Voltage/Over-Voltage Setpoints

Under-Voltage/Over-Voltage Setpoints

Under-Voltage/Over-Voltage Setpoints

Parameter

Value

Units

Parameter

Value

Units

Parameter

Value

Units

OVset(rising)

15.530

VDC

OVset(rising)

15.847

VDC

OVset(rising)

16.164

VDC

OVset(falling)

14.394

VDC

OVset(falling)

14.817

VDC

OVset(falling)

15.187

VDC

UVset(rising)

4.844

VDC

UVset(rising)

4.943

VDC

UVset(rising)

5.042

VDC

UVset(falling)

4.490

VDC

UVset(falling)

4.622

VDC

UVset(falling)

4.737

VDC

Current Limit Setpoints

Current Limit Setpoints

Current Limit Setpoints

Parameter

Value

Units

Parameter

Value

Units

Parameter

Value

Units

IR1,R2,R3 > 2ɥAmps

11.009

ɥAmps

IR1,R2,R3 > 2ɥAmps

11.009

ɥAmps

IR1,R2,R3 > 2ɥAmps

11.343

ɥAmps

Current Limit Setpoints

Current Limit Setpoints

Current Limit Setpoints

Parameter

Value

Units

Parameter

Value

Units

Parameter

Value

Units

Ilimit

3.094

Amps

Ilimit

3.125

Amps

Ilimit(max)

3.157

Amps

 

Circuit produced a fault condition when the input voltage reaches 15.1VDC, which is much less than the above set point of 15.847VDC.  If I push the reset button, this fault is repeatable at 15.1VDC.  I also noticed if I didn’t reset the IC when reducing the voltage, the fault condition wouldn’t go away until the voltage was somewhere in the range of 13V.  I didn’t write this down due to the initial trip point being way off.  So I can have the lab tech rerun this test if you feel this information is important to know.  When reviewing the data sheet, I noticed there was a falling threshold value associated with this part, which more or less causes the device to reset at a much lower value than the initial trip point.  What I am trying to figure out here is why the calculated over voltage value doesn’t fall within the over voltage trip point window from my spreadsheet?  The part is a comparator more or less so this is a little bit of a mystery.  I can simply just adjust the resistor values so the voltage is much higher than operating range and it would correct things; however, I would like to understand why the trip point isn’t falling in my calculated range.  I also ran a test on the over current protection and it did fall in the range I have calculated so that portion of the circuit is working.  Please let me know if you have any ideas here as I am going to still investigate this further by reading through the data sheet; however, I will need to know what is going on with this circuit prior to designing this into my product.

TPS1663 EVM Schematic.docx