Hi, I am trying to produce batteries with bq20z655-r1.
But while I am trying to upload my rom file to batteries, some of batteries doesnt turns chg fet on.
When I send 46x0006 or It Enable(21), chf fets turns on 2 second and turns off again. Dsg fets works normally.
Also some of batteries works normal but when I try to discharge them, chg fets stays off.
I think that the reason is CE pin. I left that pin float. Is it a problem? Do I have to pull it down?
In data flash-charge algorithm-chg inhibit threshold is 10ma and the time is 0 second. Do I have to set threshold to 0mA?
I am confused because some of batteries works normal, some of batteries works weird. Does CE pin stay unstable situation because of left float?