This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Selection of isolated flyback controller

Hi,

I'm looking for an isolated flyback controller. The specifications are as follows.
Are there any products that meet the specifications?

(specification)
Control method: Interleaved flyback
Input voltage: DC10.8V ~ DC31.2V
Output voltage: 50V to 150V
Output current: 0.34A
Switching frequency: 270kHz (with external synchronization)
UVLO: Yes
Duty: 50% or more
Feedback control: Current mode (with slope compensation)
IC power supply voltage: Starts at 12V
Current detection: Maintain at constant current (Hiccup mode is not possible)

Best regards,