This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS650830: TPS650830 power on issue

Part Number: TPS650830


Hi,

 I use TPS650830 as power solution.

LDO3V, LDO5V, VREF1V25  ramp up ,V3P3A_RTC's power level is 3.06V.



ENVR3  =3.3V, Vin=8.16V,  VPROGOTP =5V

but  VR3 is not output.

what's problem? and What's OTP load? and need write register from I2C?