Hi Team,
Customer is designing speaker application
Would you please provide recommend the buck solution for the requirement?
Requirements:
1. Vin =2.7~5.5 Max=6V
2. default vout=0.8V
3. I2C DAC 0.6~1.15V 10 or 6.25mV resolution. (6.25mV will be better)
4. PWM accuracy +/-1%
5. I2C has two addresses.
6. Maximum current above 4A
7. Efficiency 5V to 0.8V
Load= 0.1~1A >85%
Load =1A ~90%
Load =2A ~88%
Load=3A ~86%
BR,
SHH