This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCC27537: Could UCC27537 use as a MOSFET driver for 12V

Part Number: UCC27537


Hi,

I would like to know if UCC27537 can use as a MOSFET driver for 12V turn on and off?

Like as below application for fan 12V control.

  • Hi Jim,

    UCC27537 may be used for 12V fan control assuming the driver is operated within the recommended operating conditions specified in table 8.3.

    Keep in mind the driver has a 9V UVLO that will shut down the IC's output.

    Regards,

    -Mamadou