I am looking for Control IC for intermediate bus voltage circuit.
I need some function.
①Full bridge circuit control + FET driver IC integrated type
②High side floating drive, offset voltage 100V
③ Slow start
④ Overcurrent detection
[UCC28230] is similar.
But it is control + FET driver IC Separate type.
I probably use [LM5045] instead of UCC28230.
Therefore,Is it ok If LM5045 always operate with ON duty 50%?