This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TLV758P: Recommended feedback resistor example

Part Number: TLV758P

Hello experts,

I got question about FB resistor value from customer.
Could you tell me recommend FB resitor value for 5.0875V?
For example, R1=82.5k ohm +/- 0.1% , R2=10k ohm +/- 0.1% is good or not.

If you have more suitable resistor value, could you tell me?
I would appreciate if you would give me advice.

Thanks and best regards,
Ryo Akashi
  • Hi Akashi-san,

    The key to properly selecting R1 and R2 is as follows:

    So in your case, you have 82.5k+10k<=5V(10nAx100) which easily meets this requirement. 

    I hope this answers your question.