Part Number: TPS546D24AEVM
Hi there,
Could you kindly explain the test conditions as the attachment below? As far as I understand about the buck, input current is the sum of output current and IC-operating current, in that, input current is similar to or slightly larger than output current. So input current should be around 80A at full load condition in this 2PH EVM I expect from my understanding, but what the test condition presents is that the input current is typically 6.4A and 15.6A in full load (Iout = 80A). Please help my understanding. Thank you!