This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS61165: CTRL PWM control

Part Number: TPS61165

Hi Team,

Would you advise about PWM control of TPS61165 below?

In case of not using EASY scale mode,

1. Is it possible to drive the LED output current with PWM (Imax-Imin)?
2. Please let me know what the operation is for each PWM frequency of CTRL.

Thanks

Best regards,

Shidara

  • Hi Sir,

        TPS61165 can do support two kinds of dimming mode: PWM mode/Easy-Scale Mode.

        1. For PWM mode, it supports 5k to 100kHz dimming frequency and changes the internal reference with the duty cycle; the different frequency has the similar performance.

        2. For Easy Scale mode, you can refer to  Table 3 in the datasheet for the detailed reference change with different D4 to D0;

    BR

    Sean

  • Hi Sean-san

    Thank you very much for your prompt reply.

    Understood.

    Thanks

    Best regards,

    Shidara