We need to provide dual independent supply to a load.
That is 2 TPSM84624 which have input coming from different sources but connected to the same load. Both regulators will always have input supply.
But, the user selects to which regulator the load is connected.
So, by using the EN pin of one TPSM84624 to disable its output, can the output pin of that regulator be at a voltage provided by the other regulator?
Or will the internal protection circuitry come into the picture?