What is the recharge threshold value ? What is the voltage value below which when the cell goes the bms starts charging automatically?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
What is the recharge threshold value ? What is the voltage value below which when the cell goes the bms starts charging automatically?
Hi Mohit,
This depends on REG04[0] bit 0. If
Battery regulation voltage is set by REG04[7..2]
in automatic mode what is the voltage under which when battery goes the bms starts charging it?
REG04[7..2] has default value of 4.2V . According to it , the battery will start charging when its voltage drops 100mV under 4.2V??
I am confused in this part
Hi Mohit,
When adapter and battery are present, the device initiates and complete a charging cycle without software control. It automatically detects the battery voltage and charges the battery in three phases: pre-conditioning, constant current and constant voltage. At the end of the charging cycle, the charger automatically terminates when the charge current is below a preset limit in the constant voltage phase.
If adapter is still connected and battery voltage falls below 100mV or 300mV of set charge regulation voltage (depending on status of REG04[0]) it is desirable to have a battery fully charged while adapter is present. So while adapter is present, if battery voltage falls below the REG04[7..2] - 100mV/300mV thresholds then the IC will initiate charge again. The 100mV or 300mV falling threshold depends on what setting you have in REG04[7..2]. 4.2V is default.