Other Parts Discussed in Thread: BQ4050, , CSD17579Q3A, CSD17308Q3, BQ24800
I have a few questions for BQ24780S for better understanding and design optimizations. I am using the chip with a 4S battery configuration and a BQ4050 gauge and protector.
I will opeate the system with Vin max 20V and a charging/system current of max 3A.
For reference, I have posted the reference schematic of the chip below.
- Can the ACDRV, CMSRC, and BTDRV resistors (R12, R13, R28) be replaced by 5.1kOhm resistors? If no, why exactly 4kOhm?
- What is the purpose of C12 and R7? Can those components be omitted?
- Is it safe to replace all FETs (ACFET, RBFET, BATFET, High-side FET, Low-side FET) with CSD17579Q3A? This would be a more cost-effective FET that the proposed CSD17308Q3.
- As far as I understood BATPRES can be pulled permanently high. In case of battery connection, charging can still be started by setting REG0x14().
- Is this correct or do I necessarily need the hardware schematic proposed in the reference design?
- Does BATPRES need to be pulled high to REGN or 3.3V?
- I am planning to connect my 3.3V LDO to SYS and BAT bus. That means without battery, 3.3V is only available, after ACFET and RFET are on. Will this be an issue for the pins that need 3.3V (e.g. ILIM or SDA/SCL)?
- Is the cell configuration (4S) detected automatically?
- Do the input/output filter capacitors need to have 1210 footprint, or can they be 0805 with same voltage rating?
- Is the capacitor C22 on ILIM relly necessary?
- Can you give an example when I should use the independend comparator IN/OUT? Currently I have them unconnected.