This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS60401: Typical value for Rswitch (datasheet equation 1 and 2)

Part Number: TPS60401


Hi Team,

My customer is testing the TPS60401 and getting a lower output than expected. He suspected the output resistance of the converter is higher than the initial analysis. Looking to use equations 1 and 2 of the datasheet (SGLS246B, June 2004) which defines "Rswitch" as the resistance of a single MOSFET-switch inside the converter.

However, I cannot find any typical values for Rswitch in the datasheet. Could you please advise a suitable value of Rswitch? I would be happy with knowing the magnitude i.e hundreds of milliohms or tens of ohms just so that we can calculate the dominating factor of the output resistance.

Thank in advance.

Regards,

Renan 

  • Hi Renan,

    The datasheet provides the formula to calculate Rswitch value. Unfortunately, it does not give any specific range. Anything beyond the datasheet specifications is not characterized.

    However you may do a reverse calculation from the output resistance formula. From equation 1, you can see that 4*2*Rswitch is the most dominant variable. 1/(fosc*Cfly) shouldn't be more than 1/1.5 Ohm. The average is about 10/15 ohm for output resistance. But again output resistance is also dependent on VIN and temperature (As seen from figures 7 and 8).

    I hope this would be helpful in making an estimate for Rswitch. Please let me know if you need further support.
    Regards,
    Febin
  • Hi Renan,

    I hope my suggestion helped resolve your problem.

    I would like to close this thread now and please reach out to us for any further support.

    Regards,

    Febin