This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMG1210: lmg1210 with a duty cycle of 100%

Part Number: LMG1210


Hello,

 

The LMG1210 drives are intended for piloting a half-bridge structure. Its internal structure allows it to drive a hight side transistor with a duty cycle of 100%?

The driver is powered on the logic part and has an isolated and floating power supply directly between the HB and HS input.

 

Here is an example of an application diagram.

 

Thank you for your help.

 

Cordially