Part Number: TPS23861
Hi Team,
when i have two TPS23861 also A3 pin that both to low ( the default address is 0x20), how do i set the address of the second TPS23861.
thanks for your help and looking forward to reply.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TPS23861
Hi Team,
when i have two TPS23861 also A3 pin that both to low ( the default address is 0x20), how do i set the address of the second TPS23861.
thanks for your help and looking forward to reply.
Hi Tommy, this is currently being looked into and an answer will be posted when available. Thanks!
Hi Tommy, you want to have a similar connections like the TPS23861EVM-612. AOUT in the first PSE is connected to AIN in the second PSE. AIN in the first PSE is floating and AOUT in the second PSE is floating.
Also note A3 in the second PSE is left floating. Please let me know if this helps. Thanks!