This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ24086: About TS pin

Part Number: BQ24086


Hi,

Could you tell me about TS pin ?
Customer wants to install a ceramic capacitor to deal with noise on the TS pin.

1. EVM is set to 0.01 μF.
 What is the maximum capacity that can be installed?

2. Is the management by the TS pin a non latch type?
 When the temperature returns to the set range, it automatically returns and STATUS also returns.
 Is this understanding correct?


Regards,
Yusuke

  • Hi,

    Is there any update about questions?
    If there is any progress please contact me.

    Best regards,
    Yusuke

  • Hi Yusuke,

    What is the maximum capacity that can be installed? What capacitance value were you considering? We don't typically provide a max capacitance value for pins, recommend using value close to what is in evm.

    Is the management by the TS pin a non latch type? The suspend mode is entered when the pack temperature is not within the valid temperature range. During the suspend mode, the charger is set to OFF, but the timers are not reset The normal charging mode resumes when the pack temperature returns to the valid temperature range. 

     


    Best,