Other Parts Discussed in Thread: BQSTUDIO
Hello,
I have a question regarding /SHUTDN pin functionality of BQ40z80.
I have pin 17 assigned as /SHUTDN and button to GND connected to it.
The User Guide says:
When a high-to-low transition on the SHUTDN pin is detected with a debounce delay of about 1 s for the low level threshold, the gauge turns off the CHG and DSG FETs immediately
However what I observe on the pin during normal state is low level actually (when the button is not pushed). Does I need to add externall pul-up to VCC?
Regards,
Adam