Other Parts Discussed in Thread: LM5069
Hello,
we want to use the LM5060 to switch off the motor power when the current flow to the motor exceed a defined current (let us say 23 A) for a defined time (let us say 2ms).
In the Forum I have seen a problem from another user, that the LM5060 has problems with short circuits on output side.
In my application we must also calculate with schort circuits on output side and we must switch off the output in a safe way imidialtely.
I want to protect the VIN input with a diode from input voltage to the VIN input and a capacitor from VIN input to GND. This shall hold energie to let the LM5060 operate to switch of the MOSFET.
In the data sheet i can not see that the LM5060 will operate when the VIN voltage is less than the SENSE input voltage and the output voltage.
I would assume that this will work, but i want to ask if some experience exists if this will work.
Would be happy abou a fast response.