Part Number: LMZ22005
Other Parts Discussed in Thread: TPSM84824, LMZ31710, LMZ31520
Hi!
Can LMZ22005 be used in parallel mode for more current capacity?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Ser,
The LMZ22005 does not have any current sharing circuitry to help ensure modules are sharing the load current evenly. We do have other modules that would be better suited. What is your overall input and output voltage and current requirements?
Kris
Hi Ser,
The TPSM84824 still meets same or similar MSL (moisture sensitivity level) ratings as some of our overmolded modules like LMZ31520 and LMZ31710, and even allows higher peak reflow temperatures than these other devices mentioned.
In terms of manufacturing/soldering considerations for power modules, take a look at this app note on the topic.
Ser,
Applying a heat sink to the inductor should be fine. Be careful to avoid contacting the leads on the sides of the inductor with the heatsink. What are your design conditions such that you foresee need for a heatsink?
Kris