This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ40Z80EVM-020: bqstudio and MCU command control mismatch

Part Number: BQ40Z80EVM-020
Other Parts Discussed in Thread: BQ40Z80, BQSTUDIO

Hi team,

My customer now use our BQ40Z80EVM in their vacuum robot 4S BMS project.

They send cell voltage read command to BQ40Z80 via bqstudio, and the data read back is correct.

But when the device is reset, then they use their MCU to send the code 0x0071 to read the cell voltage message, the data read back is incorrect.

Besides, if the device is reset, and first time read is executed by bqstudio, then send 0x0071 to BQ40Z80, the read back data is back to correct.

There is another issue:

When they use bqstudio, all operation is correct. But after reset, and first read operation is executed by bqstudio, then they can use 0x0071 command to read back cell voltage. But they send 0x0072 and get back wrong data.

Can you please help me with these two issue? Is there any command need to be sent after the reset?

Thanks for your help.

Gary