This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS1H000-Q1: Is the 10K ohm series resistor between TPS1H000-q1 and MCU needed

Part Number: TPS1H000-Q1

I see a 10K resistor in IO lines between MCU and TPS1H000, even on an open-drain output. Why is this resistor needed? And why does it need to be so high in value?

  • Hi,

    Welcome to E2E!

    The 10-kOhm resistors on the IO lines are to help protect the MCU, specifically 5V. If the MCU is 3.3V based, we recommend a 4.7-kOhm resistor. 

  • Hello,

    The TPS1H000-Q1's IOs as well as your MCU IOs have ESD and body diodes. When you have transients like ISO pulses or loss of battery/ground you can potentially have positive voltage spikes around the GND/IO pins. Without a current limiting resistor there the ESD diodes may forward bias and break down in these situations. The 4.7k for 3.3V and 10k for 5V  make sure the IOs receive the correct logic level across all factors like temperatures and tolerances.