This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS61023: Fail analysis

Part Number: TPS61023

Hi sir,

My PCB-ASSY is in fail status after SMT.

My input 5V, max current 1.4A,output voltage about 5.5v.

Since this device have functions of OVP, OTP, OSP, UVL,

So I think it’s difficult  for broken.

Now the fail status is input short between VIN and GND,

What’s the problem?

Why this device is broken?

Can you provide any suggestion on probability or reason?

BTW, if the input voltage is fluctuating around UVLO for a long time, is this can case failure?

Tks,

Regards,