This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS61170: Output capacitor value

Part Number: TPS61170

Hi,

The recommended value of the output capacitor is specified as Max 10μF.
According to the customer's evaluation, it was found that the electrolytic capacitor 470 μF improves the noise.
So they are trying to connect this capacitor, is there a problem?
I think it is okay if the large capacitor is placed after the FB point, is it correct?

Best regards,
Yuto Sakai