This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ78350-R1: Production tool

Part Number: BQ78350-R1
Other Parts Discussed in Thread: EV2400

Hi,

I just saw, there is a software for production. Where can I download it?

Thanks in advance

  • Hi Paul,

    I sent you an E2E connection request. Accept the request an send me a quick note and I will send you the link to download the production software available.

    Best regards,

    Matt

  • I did download the updater, but I have only the EV2400, so I can not use production tool, right?

    So I would like to have the following kind of process:

    1) Program Srec

    2) Write serial number

    3) Seal the device with individual, non standard key.

    Do you offer some kind of tool, which can cover these steps? Or do I have to use multiple tools?

    If not, What would be the alternative? Is there some kind of DLL and API to make my own program and control the EV2400 ?

  • Hi Paul,

    I sent you the link to one more resource which is example code to write the srec using the EV2400. I also sent you the contact info for two 3rd party vendors that may be able to help create a production solution if you need help.

    Best regards,

    Matt