Other Parts Discussed in Thread: UCC28740, UCC28780
If I want to use UCC28740 as Flyback controller, and use the LMG3410R050 to replace the MOSFET, to make the solution smaller. Is it possible and anything that needs to be considered?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
If I want to use UCC28740 as Flyback controller, and use the LMG3410R050 to replace the MOSFET, to make the solution smaller. Is it possible and anything that needs to be considered?
Hello,
As far as using the GaN for Flyback topology, I don't see problems. You may post this question to the controller part number and check with the controller expert to see if it is suitable.
Some customers are using UCC28780 with LMG3410 device for Active Clamp Flyback topology.
For designing with GaN, some guidelines for PCB layout are:
To minimize the power loop for lowest parasitic inductance:
For better thermal performance it can also follow our general design rules as multi-layer board:
When the power loop is minimized, the voltage ringing can be reduced and GaN Fet will have a better slew rate, which allows applications to take advantage of GaN.
Hi Yichi,
Thanks for your support.
I will take UCC28780EVM as reference.
After check the EVM schematic, there‘s an additional question:
The Flyback controller and GaN are powered by the voltage Pre_bias, which is generated by the auxiliary winding.
When AC power on, the auxiliary winding may not be able to provide the voltage Pre_bias. And I didn't see any resistor from VBULK to Pre_bias.
So how the Flyback controller can be powered when AC power just on, can you kindly advise me, thanks.
Hello User4542981,
Thank you for your interest in the UCC28780 Active-Clamp Flyback controller.
The UCC28780 does not require a start-up resistor to Vbulk because this function is provided by the Vsw-sensing transistor Q2 through the SWS pin. This is explained in the UCC28780 datasheet, Section 7.3.3 (VDD Pin) and follow-on Sections 7.3.5 (HVG and SWS Pins) and 7.4.8 (Start-Up Sequence).
Kindly read through the datasheet to understand how this controller works.
Regards,
Ulrich