Other Parts Discussed in Thread: UCC28700
Is UCC28630 appropriate for this wide input operation?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
I found a reference design using the UCC28700 for a 25V to 500V input range with 28V output. This is a 10 W design. This could be used up to a 60 W design by changing the transformer.
The UCC28630 uses a similar control law and it may be possible to get this device to work in this application as well.
Regards,
Mike
UCC28630 has narrower overvoltage - undervoltage band. I mean; UCC28630 UVLO thresholds on/off (V) 14.5/8 , while ucc28700's is 21/8V. So I believe it can't go that far. I think current controllers are better option.
Thanks, I'll try but I wonder why webench is limited to 85VAC minimum input?