This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCC256404: Burst Mode correlation to secondary output and maximum soft start capacitor

Part Number: UCC256404

TI Team, 

We are using the UCC256404 in a design and have some questions- two of which are below:

  1. Is there a way to correlate the BMTH threshold setting to output power/current/voltage or similar? Because it is for an audio product, our design runs at very low power most of the time (<30W) but the SMPS has the capacity to run continuously at 145W as required for maximum continuous volume. A BMTH threshold of "0.6" as shown in the data sheet example doesn't offer any way to correlate at what condition on the secondary side we will enter into boost mode.
  2. Any thoughts on how to extend the soft start period to several hundred milliseconds? We have a significant amount of bulk capacitance on the output rail to help with transients. Currently, the LLC hits the OCthreshold and sort of "hiccups" until it gets that capacitance charged. I would like to extend the softstart time (we can handle the delayed start without issue) to a longer period of time- but it seems maybe that the highest value capacitance we can use for the soft-start capacitor is 470nF. We can adjust the RLL upper and lower, but to get the sort of time frames we're after, we end up with several mega-ohm resistors. 

Thanks in advance,
Cody