Hi,
Does TI have an alternative to ADP5310 ? It's an ultra low power buck converter that can be changed between hysteresis and PWM modes depending on the power required by the load. e.g. a microcontroller that is in and out of sleep.
We found ADP5310 because we have used ADP5300 in a previous product (similar to ADP5301 / ADP5302 / ADP5303) but the new product has a much higher battery voltage (9-14V).
ADP5310 is a very impressive SMPS and the only one in our list that can support our battery voltage, but we don't like that it's a multichannel part. This will make it extremely difficult to replace if it were to become obsolete.
We don't really need to be able to manually switch between hysteresis and PWM modes, but we do need great efficiencies when < 1mA and when > 50mA.
Kind regards,