This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ2980EVM-883: installing another chip

Part Number: BQ2980EVM-883

Hello


Our team is developing a board with a very small battery capacity (about 100mA / h). Lipo battery is used. To protect it from a full discharge, we need a protection circuit. I noticed your BQ298010 chip. I think it should help us.
but before adding it to the circuit, we would like to check its operation and make sure that this is what we need.
I found the BQ2980EVM-883 board on your website. but on the board set other chip with a cut-off threshold (UVP) of 2.6 volts. this is too low a threshold for Lipo.
I have a question: can you install the BQ298010 chip on this board? or does this board ship as is?

Best regards, Sergey.