Other Parts Discussed in Thread: TPS544C25, CSD85301Q2, CSD87331Q3D, CSD87381P, CSD87588N, CSD87350Q5D, TIDA-01393
Hi
The datasheet of TPS650864 shows some power map examples.
One of them looks like as below.
In this configuration, TPS544C25 is used to supply VCCINT to FPGA.
While we should connect VCCINT to BUCK2 output if these are same voltage level.
1. In this power map, TPS544C25 is used to supply 0.72V which is different voltage level with VCCBRAM.
The purpose of TPS544C25 implemented is just to supplying different voltage with BUCK2, isn't it?
2. Assumed VCCINT and VCCBRAM are same voltage, would the current into VCCINT and VCCBRAM which are same voltage depend on ext FET? (Additional power regulator is not needed?)
BestRegards