Customer is reviewing External Gate Resistor Design Guide for Gate Drivers app note to figure out the resistors they would need on the LMG1020EVM-006 and they are not getting a good answer. In looking at the spec for the EPC2019 data sheet, it notes a Ciss of 200pF.
Attached are scope traces, blue is the K testpoint, green is enable and the yellow is gate voltage. You can see when turning the FET off it has huge swing, I measure this to be 426 MHz. So from the app note and equation 1, I get an inductance of 0.7nH. If I compare that to their example on the second page, Ciss of 9250pF and frequency of 3.57 MHz, they get 2149nH of inductance. This seems to me to be too large of a difference between the 2 examples.
Any ideas?
Regards,
Mark