Other Parts Discussed in Thread: LM3445, LM3444, LM3414HV
Hi E2E,
Good day!
Can we set the LED current of this part lower than 150mA, specifically 40mA?
Best regards,
Franz
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello Franz,
According to the datasheet: "To ensure stability, RIADJ must be less that 30 kΩ, implying a minimum ILED of 50 mA can be programmed. The
tolerance of ILED of 150 mA is shown in the ELECTRICAL CHARACTERISTICS."
It's close, however operating out of the recommended range can lead to issues.
Do they need common anode?
Best Regards,
Hi Irwin,
Yes, is there any common anode constant current LED driver that can support 40mA current setting?
Best regards,
Franz
Hello,
The LM3445/LM3444 are controllers that could do this, they were created for a different purpose but are fairly simple parts to use.
What is your input voltage, output voltage and any other relevant information for this design?
Best Regards,
Hi Irwin,
Thank you for your response.
Input voltage would be 18V to 32V and will have 1 to 5 LEDs connected.
Best regards,
Franz
Hello Franz,
The LM3444/45 should work, just have to generate a voltage for VCC. Also, if you go this route make sure that you meet the minimum on-time requirement since you will have low duty cycle with 1 led and 32V input.
You can look at those part's datasheets. The circuit will be reduced from what you see since these were meant for off-line. I've worked with these parts quite a bit if you need direction.
Best Regards,
Hi Irwin,
Thank you for your suggestion. Will check this part.
Best regards,
Franz
Hi Irwin,
Good day!
Just a follow-up inquiry on this. Is LM3414HV capable to be used with 40mA LED current?
Best regards,
Franz
Hello Franz,
In the datasheet I see an output range of 0.35A to 1A for setting LED current. There is also an analog dimming/foldback method that can take a 1A set point down to 0.1A. I don't see anywhere where this can be used below this. I wouldn't recommend trying to regulate current at 40 mA with this part.
Best Regards,
Irwin