This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS54061: TPS54061 ocp behavior

Part Number: TPS54061

Hi Team,

Customer have some question about TPS54061 OCP behavior.

Test condition:

VIN = 24V, Iload = 0.1A ~ 0.4A. T = 1ms, 50% duty, slew rate : 32mA/us

Questions:

1.When the output load are 0.1A, why device stop switching?

2. The waveform shown sw node switching but output drop. Any possible reason? 

Waveform:

Shaq