Other Parts Discussed in Thread: LM317M
Hi,
We are using "TL5209DR" in our design and below is the design
1.Vin =9V
2.Vout = 5V@500mA expected
3.Cout =10uF,0.1uF
4.Cin = 1uF,0.1uF
5.CBYP = 470pF
6.R1 = 100K ,R2 = 300K
Please confirm if the above design works as per our requirement of 5V output voltage @0.5A. It is mentioned in the datasheet that the dropout voltage at 500mA is 500mV.We are supplying input voltage of 9V and the expected output voltage is 5V and there is a headroom of 4 V between input and output voltage.If the system operates at full load(500mA) what is the expected output voltage.Is it 5V constant or will it be 4.5V(need to consider drop out?).Kindly clarify how the drop out should be considered?