This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
That is correct, if VCOM_CTRL is pulled up to the battery or IO supply, the VCOM active discharge would never be enabled. The input logic low threshold for VCOM_CTRL is 0.4 V, much lower than the device UVLO of 2.9 V. In this case, since the internal discharge feature is not used, it's recommended to leave VCOM_DIS floating.
If discharge is still desired, an external resistor could be connected from VCOM to GND, but please keep in mind the VCOM drive current capability specified in the datasheet.
Thanks,
Gerard