Other Parts Discussed in Thread: BQ7716
Dear TIers,
I am using a BQ77915 in my design and would like to implement an independent secondary level of protection through bq7716xy. I am trying to minimize as much as possible the sleep current while the battery is disconnected from my load, and it looks like the two combined would get me roughly a maximum of 5uA sleep current.
I assume I only need to branch these two devices off of each cells but I wanted to double check that there are no measurement interference between these two devices I would need to handle ?
Thank you!