This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ24600: Charging is not done with its set charge current

Part Number: BQ24600

I have designed Li-ion Battery Charger using BQ24600. I have used 1S6P battery Configuration. 

Battery is getting charged by only 250 mA current, while set charge current is 3A. state LED is contentiously Glow, which indicates charging is going ON but not at set charge current. 

What is possible reason for not charging at 3A?