This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS7B63-Q1: Extend WD time longer than 500 ms

Part Number: TPS7B63-Q1

Can I choose a larger resistance and extend the watchdog time to more than 500 ms?

  • Hi Clark, 

    Technically, yes, a higher than 200K Ohms resistor could give you a higher watchdog clock cycle, but the tolerance of the cycle will get higher than 15% as well. As you can see, we only have tolerance data up to 500ms for the WD timer. How much does your customer plan to set it to?

    Regards, 
    Jason Song

  • Jason,

    In this application, they would use the watchdog to wake up part of the system about every 2 seconds, unless the WD was reset.  I think the expanded tolerance would be acceptable; precise timing is not a requirement.

    Thanks!

  • Hi Clark, 

    Understood, thanks for providing the update. I would advise the customer to try their usage case with the EVM and to see if the expanded tolerance would meet their requirement. If you need additional assistance, please don't hesitate to contact me back. 

    Regards, 

    Jason Song