I am reviewing a design that uses TPS43060 to create 50V from 28V nominal (24 to 32V) with a max output current of ~7A. When I input these parameters into Webench, I don't see TPS43060 as an option. I am concerned that the TPS43060 doesn't support a high enough voltage for this application. Is this correct?