This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ2970: Please ask which model of BQ297xx series supports the 0v forbidden charging function?

Expert 2630 points
Part Number: BQ2970

Please ask which model of BQ297xx series supports the 0v forbidden charging function?

  • Hi, 

    Please refer to datasheet below:

    9.4.7 0-V Charging Inhibit Function This feature inhibits recharging a battery that has an internal short circuit of a 0-V battery. If the battery voltage is below the charge inhibit voltage V0INH or lower, the charge FET control gate is fixed to the Pack– voltage to inhibit charging. When the battery is equal to V0INH or higher, charging can be performed. The 0-V charge inhibit function is available in all configurations of the BQ297xx device.

    Regards, 

    Sandy