This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM2585: About the internal logic.

Guru 11255 points
Part Number: LM2585

Hi team.

I have some questions about the internal logic for LM2585.

My customer refer to snva005b(p.7) and configure the flyback.

1. About the soft start.

   If a momentary power failure occurs and the input voltage has a residual voltage of several V, will soft start start if the input voltage is restored even if the COMP pin voltage is 0V?

 I think soft-start will not restart unless the device is turned off.

2. About the control logic for SWpin.

    I'd like to know about the movement for SWpin.

    Does the logic movement for FB(COMPpin) match below?

3. If you have something document about the movement for internal logic, could you share us?

    I would like to know the logic control for the movement of each comparator.

Sincerely.

Kengo.